Methodology
To work out the estimated amount of bottled water each city buys every year, we used data from London Gov which claimed that 7.7 billion plastic water bottles are used in the UK each year.
Using data from a recent report from One Less Bottle, 175 bottles are used by Londoners each day. We then calculated this for the total London population by multiplying this figure by the capital's population, and divided the remaining UK population per city using population data from Nomis to work out how this figure is estimated to be proportioned out per capita to calculate each city's estimated plastic bottle usage..
We then ranked these in order of size to show a comparison of the height of the plastic problem in each city. This has been ranked purely on a population basis and is in no way suggesting that any city is contributing to plastic pollution the most, it is to visualise the countrywide plastic problem to make Brits think about their plastic consumption.
Asset methodology:
London:
To get the figure of 890, we found that the River Thames measures 215 miles in length. We then converted this into centimetres which we then divided by the average height of a 500ml water bottle (20cm) to find out how many bottles fit the length of the Thames. We then divided London’s plastic consumption by this figure to get the result (1,539,952,400/ 1,730,044.8).
Birmingham:
To get the figure of 446,287, we used the height of the Bullring (54 meters) and divided it by the average height of a 500ml water bottle (20cm) to find how many bottles are the height of the Bullring. We then divided Birmingham’s plastic consumption by this figure to get the result (120,497,570 / 270).
Leeds:
To get the figure of 247,694, we used the height of Leeds Town Hall (69 meters) and divided it by the average height of a 500ml water bottle (20cm) to find how many bottles are the height of Leeds Town Hall. We then divided Leeds’ plastic consumption by this figure to get the result (85,454,397/ 345).
To get the figure for the amount Brits spend on Bottled water:
We used source 1 which indicated that 7.7 billion single-use plastic water bottles are bought in the UK every year. We then used the population of the UK (67.33 million) which we used to find the estimated number of plastic water bottles bought per person in the UK. This figure (114) was then multiplied by ONS’s latest figures on the cost of bottled mineral (£2.15) water to give a figure of £245.