5 Awesome Christmas Dinner Leftover Recipe Ideas
There's always leftovers from your Christmas dinner. Here are some delicious ways you can use your leftovers instead of throwing them down the disposer.
Want to use this infographic on your site? Just copy the code below into your CMS.
The only thing more stressful than having to prepare a Christmas meal, is dealing with the inevitable clean-up operation that follows. Every year, you’ve eaten well and just want to get on with enjoying your presents, but for the mountain of food that demands your attention. Sure, some can be put away for later, but few fridges are prepared to cope with the sheer volume that needs dealing with.
Therefore, a little prep work can go a long way towards a stress-free post-lunchtime on Christmas Day. We hate food waste at InSinkErator, and think that it’s a great shame to see any part of the meal you worked so hard over get tossed unceremoniously, so here’s a list of recipes using your leftovers that we think can prove useful.
The quantities listed are for the respective number of servings, meaning that they can be adjusted as needed. With these in mind, you shouldn’t even need to hit up a supermarket before New Year’s, and can enjoy the festive period indoors where it’s nice and warm.
Be sure to use one of our food waste disposers for anything that doesn’t get used in these recipes to help minimise food waste which will otherwise end up at landfill this Christmas.
Want to speak to a member of our team? We’re here to help